If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Beijing, China - Caterpillar Oil & Gas will unveil latest innovative power solutions for the Asia Pacific region at the 17th China International Petroleum and Petrochemical Technology and Equipment Exhibition (CIPPE), to be held March 20-22 in Beijing.
New Cat® products and technologies featured at this year’s exhibition include Cat ConnectTM for fleet management, a Cat C15 diesel generator set with Product Link installed, Dynamic Transmission Output Control (DTOC) to enhance well service operations and Cat Electric Motors for gas compression.
“Cat Connect catches emerging technical problems early before catastrophic failure, identifies optimization opportunities and recommends configuration improvements, giving our customers the power to stay ahead of the competition. We’re very excited and look forward to demonstrate the features and benefits of Cat Connect, DTOC and other best-in-class products to all CIPPE attendees in person at this year’s show.” said Alan Zhang, Caterpillar Oil & Gas Asia Pacific China region sales manager.
These new Cat products and technologies include:
Cat Connect. Cat Connect combines technology and services to boost your operational efficiency. With just a few clicks, it helps you take the guesswork out of equipment management by monitoring, managing and enhancing all connected Cat equipment operations remotely through Product Link, Cat Productivity Optimiser and Advanced Condition Monitoring in four key areas:
Cat Electric Motors. Cat electric motors are of the AC induction type and built for low vibration and high rigidity, so you get great performance over a long, productive life. Standard features include hazardous location ratings and a high strength alloy (AISI 4140/ DIN 42CrMo4) forged, keyless shaft. Order board is now available for 50Hz models.
Caterpillar Dynamic Transmission Output Control (DTOC). Caterpillar DTOC technology is the answer to well service operations that typically have to be done manually. It is compatible with current production Cat transmissions, can be integrated on a variety of control systems and is intuitively easy to manage by any experienced well service operator through three key automated functions:
1. Automated Stall Test Mode (ASTM) - Designed for pressure testing, ASTM reads torque output and automatically sets gear and engine speed to achieve desired pressure without pressure spikes.
2. Automated Speed Control (ASC) Manual-Shift - ASC allows operators to adjust flowrate while in gear and the engine automatically changes speed. It is extremely useful during cementing, as it allows pumping at extremely low flow rates that are not possible in direct drive.
3. Automated Speed Control (ASC) Auto-shift - Operators input desired flow rate and DTOC automatically changes engine speed and gear to obtain the desired flow.
For more information on the solutions and services Caterpillar Oil & Gas offers, please visit www.cat.com/oilandgas or stop by the Caterpillar booth in Hall W1, Booth W1503, to meet with one of our Oil & Gas industry professionals.
# # #
About Caterpillar Oil & Gas
Caterpillar Oil & Gas, Caterpillar Inc.’s oil and gas division with headquarters in Houston, Texas, consolidates all the sales and service activities for Cat oil and gas power solutions. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides premier power solutions with outputs from 31 to 16,000 kW. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at: cat.com
About Caterpillar :
For over 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2016 sales and revenues of $38.5 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Construction Industries, Resource Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
©2017 Caterpillar
All Rights Reserved
Press Inquiries |
Sarah Pullen Phone: +1 309 675 1513 |