Beijing, China – Caterpillar Oil and Gas is pleased to announce a China Non-road (NR) Stage III 3,000 hp power module for the pressure pumping market. “SANY Oil Intelligent Equipment (SANY Oil) received this innovative package by the local Cat® dealer LSH North in March of 2018 and will display a well stimulation truck using this technology at the CIPPE oil show in Beijing,” said Alan Zhang, China regional manager for Caterpillar Oil & Gas. “This power module includes a 3512E engine together with a CX48-P3060 transmission offering a full Caterpillar well stimulation solution to solve China pressure pumping customer demand for higher power density.”
Caterpillar was the first engine manufacturer to earn NR Stage III certification for well stimulation engine in China in October 2015. SANY OIL will utilize this power module to produce a 4-axle pressure pumping truck that complies with road limits related to per axle weight and will be operational by 2Q 2018.
“Caterpillar has a long history in well stimulation engines and transmissions,” said Rodney Harms, well service manager for Caterpillar Oil & Gas. “Our experienced team has a deep understanding of tough pressure pumping operations and customer requirements and the new 3512E was designed with those needs in mind. The engine is based on the U.S. EPA Tier 4 engine platform, with improvements that enable the engine to reliably meet the increased power density and emission standards of China NR Stage III. The transmission leverages decades of transmission design and over 10 years of proven durability on the TH55 to deliver a tailored solution for pressure pumping,” said Harms.
With China’s new road vehicle GB1589/2016 regulation, all new well stimulation trucks must meet the “per axle load” limitation and the maximum height limitation. Caterpillar’s launch of this light weight, compact module is targeted to meet these regulations with the highest power density engine transmission package available. By utilizing the Cat power module, customers can continue to use the 4-axle chassis to build the 2500 type pressure pumping trucks without exceeding the axle loads or vehicle height limitations of the new regulation.
The 3512E engine combined with the CX48-P3060 transmission deliver an ideal high-density power solution for well stimulation operations at the lightest weight in its class. “Whether operations reside in mountainous areas or desert terrain, this package can accomplish more than the 5-axle truck or other heavy vehicles which are unable to handle the rough terrain,” states Harms.
With Cat Connect, technology embedded into the equipment, customers can make well-informed and timely equipment management decisions to help control costs, improve operations efficiency, optimize production and reduce downtime and risk. To learn more about Caterpillar’s well stimulation power module and meet the product experts, stop by the Caterpillar exhibit #W1501 at CIPPE to be held 27 to 29 March 2018 in Beijing, China.
About Caterpillar Oil & Gas
Caterpillar Oil & Gas, Caterpillar Inc.’s oil and gas division with headquarters in Houston, Texas, consolidates all the sales and service activities for Cat oil and gas power solutions. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides premier power solutions with outputs from 31 to 16,000 kW. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at: cat.com
About Caterpillar
For over 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2017 sales and revenue of $45.5 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Construction Industries, Resource Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
©2018 Caterpillar
All Rights Reserved
Press Inquiries |
Sarah Pullen Phone: +1 309 675 1513 |