Hamburg, Germany – Caterpillar Marine is pleased to announce that the Spanish shipping company Baleària, will be converting three ferries from Diesel to LNG dual fuel using Caterpillar and MaK solutions. Caterpillar Marine dealer Finanzauto will perform the engine conversion, with work on the ships scheduled to begin in early of 2019.
Ettore Morace, General Director of Operations at Baleària, pointed out that this conversion project supports Baleària’s goal to reduce emissions significantly and provide clean transportation. By using MaK DF engines Baleària will virtually eliminate the sulfur and particulate matter in the exhaust gases, while also cutting down NOx, resulting in even lower CO2 emissions. This will help Baleària to have a state of the art and eco-efficient fleet.
The three ferries named Abel Matutes, Bahama Mama, and Martin i Soler, are currently equipped with two MaK 9 M 43 C main engines. After the conversion, the vessels will operate on two MaK 9 M 46 DF engines, which has a rated engine output of 8685kW. The MaK engines are used in a control pitch propeller application with a gearbox. The conversion will allow the engines to be powered by gas.
Caterpillar will provide DF-Engine conversion kits and all the required engine modules including an ignition fuel oil module, engine ventilation modules, an exhaust gas ventilation module, GVU ventilation modules, and gas valve units with housing.
Caterpillar Marine has already successfully converted engines for other companies as well. Caterpillar worked with Cat dealer Bolier to perform an engine conversion for the Coral Anthelia from a MaK 6 M 43 C to an MaK 6 M 46 DF engine. An engine conversion was also performed with Caterpillar dealer Pon for the Fure West, converting the MaK 7 M 43 C to an MaK 7 M 46 DF and delivered a gas system.
Included in their planning to expand and renew their fleet, Baleària will also replace the existing main engines on board their high-speed ferry ‘Jaume III’ with four new Caterpillar 16-cylinder C280 propulsion engines; each engine delivers 5650 kW at 1000 rpm. A similar repower was done back in 2017 on board the sister vessel ‘Jaume II’ resulting in a notable increase in efficiency and service, with the ship being able to reach high transit speed.
About Caterpillar Marine:
Caterpillar Marine, with headquarters in Hamburg, Germany, groups all the marketing and service activities for Cat® and MaK marine diesel, dual fuel and gas power and propulsion systems within Caterpillar Inc. The organization provides premier power solutions in the medium- and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100 kWe in marine generator sets as well as a comprehensive portfolio of propulsion solutions. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are.
More information is available at: www.cat.com/marine
About Caterpillar:
For 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2017 sales and revenue of $45.5 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Construction Industries, Resource Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
©2018 Caterpillar
All Rights Reserved
Press Inquiries
Danielle Wills