How To Choose The Right Cat® Ground Engaging Tools

Estimated read time: 8 minutes

One way to increase your equipment’s effectiveness is to pick out the right Cat® ground engaging tools (GET) for your machine and application. The right bucket or blade and ground engaging tools together also can improve operational outcomes. Invest only in what your job and application need, not what works for someone else’s operation.

In addition to boosting productivity, efficiency and cost savings, the right GET can:

  • Help improve performance. Ground engaging tools are designed to penetrate and move material, which can help boost machine performance.

  • Expand equipment versatility. With a wide range of options, you can choose different GET for the same machine to expand versatility on the job. You can select different tips and edges to support specific projects, and you can change ground engaging tools as many times as you need. Cat GET systems are easy to change, which saves time between tasks and helps you complete jobs faster.

  • Provide extra protection and longevity for valuable equipment. Having the right bucket and knowing which GET you need for your bucket protects the machine structure from damage, helping to extend its longevity. GET helps absorb impact when it makes contact with the ground, which protects the machine’s internal components from excessive force. A GET system can also indirectly help reduce corrosion-related damage because it acts as a “sacrificial layer” that absorbs wear and tear from abrasive materials. This helps to reduce the exposure of the bucket’s base metal to moisture and corrosive elements.

  • Improved productivity and uptime. Increased machine efficiency means less time spent on tasks. When your machine digs faster and easier, you spend less time on each task and reliably meet deadlines or complete them ahead of schedule.

  • Lower operating costs. You can expect fewer repair costs when you fit equipment with the right GET for the application and material. GET impact absorption reduces wear on buckets and other components resulting in fewer parts replacements.

of

How to Choose Cat Ground Engaging Tools

The first step in selecting ground engaging tools is to consider the needs of your typical machine work. Next, determine your highest priorities across jobs.

Do you need to control fuel consumption, save time spent on tasks or protect a valuable machine? Prioritizing your needs will help you determine which GET to choose as you work through each of the selection steps that follow.

Match GET To The Application

According to Tilak Inturi, senior parts and services consultant (GET), “The process starts with the right bucket on the machine for the application. GET won’t compensate for a poor bucket choice. The bucket and GET need to work together to deliver the best solution.”

Matching bucket and GET to the specific task at hand will help deliver maximum efficiency and productivity. Consider the following factors to make the right choices for your next job:

  • What type of work will the bucket be performing?

  • Will it be used for digging, grading, loading or something else?

  • What type of material will the machine be working in?

The answers to these questions will guide you in choosing the right heavy equipment attachments. For example, attachments with general purpose teeth are great for loose soil and aggregates. But if the job involves breaking through hard material, you might need a more aggressive tool like a ripper shank or a heavy-duty bucket tooth.

   

The process starts with the right bucket on the machine for the application. GET won’t compensate for a poor bucket choice. The bucket and GET need to work together to deliver the best solution.

Tilak Inturi

Senior Parts and Services Consultant (GET)

   

Match The Tools To Your Machine

Smaller machines require compact, lighter attachments to prevent tipping or equipment strain from increased weight. Larger machines can handle heavier tools, but you should still check the equipment’s weight capacity before choosing an attachment. It’s also essential to factor material density and weight into the total weight to ensure your equipment can handle the attachment and the loads it handles. You should also consider the machine's maneuverability, especially if working in tight spaces or uneven terrain.

Evaluate The Material Type

Different attachments and equipment models offer various levels of durability working in different types of material. Depending on the material, you should choose GET components that will deliver the longest wear and productivity in your application. For softer materials like loose soil or aggregates, general purpose teeth might be adequate. However, you might need to consider GET with higher abrasion resistance, longer wear and strength for harder materials such as rock or frozen ground.

Why Your Choice Matters

Buckets or blades, tips or edges, rippers or side cutters — no matter the size, attachments and GET are the main reason that machine is on the job. Your ground engaging tool selections have a direct impact on the machine’s ability to produce. Improper selection could lead to:

  • Higher fuel consumption from adding components that are larger and heavier than needed.

  • Reduced engine and power train life from added stress on the machine.

  • Increased operator fatigue from struggling to operate the machine, cab vibration and more time required to complete tasks.

  • Increased contact surface. The larger the contact surface, the more stress on the system. This increased resistance requires the machine to work harder, which could result in:

    • More fuel consumption
    • Increased time taken to move the material
    • Inefficient penetration, digging or loading
of

GET Options By Machine

Excavators

Excavators are the most versatile machine on your jobsite. Cat offers a wide range of choices to match your excavator, its bucket, the application and material. Here’s a snapshot you can review with your Cat dealer:

  • Four standard bucket styles: general duty, heavy duty, severe duty and extreme duty

  • Tips and adapters:

    • K Series hammerless system
    • J Series options
    • Four CapSure™ options
  • Bucket front edge protection:

    • Base edge systems: bolt-on, straight and spade
    • Base Edge End Protection (BEEP)
  • Side and edge protection:

    • Sidebar protectors, side cutters, half arrows, segments and top covers

Dozers

Dozers move ground on construction sites, residential developments and hundreds of other places. A dozer’s main work tools are a blade and a ripper. The universal blade is curved, wide and tall so that it can carry material. Other blades are flat or shorter, but they all do a similar job: leveling the ground. The ripper loosens the rocky or compact earth, which makes dozing or loading easier.

Options include:

  • Cutting edges and end bits

  • Sidebar protectors

  • Complete ripper systems with tips and shank protectors

Motor Graders

Caterpillar offers various cutting edge options suitable for different applications.

Unique offerings like the Cat GraderBit™ system meet the toughest application needs and are complemented by multiple end bit options. Trust your Cat dealer to offer you solutions that focus on total machine productivity.

  • Cutting edges: general duty, through-hardened and Tungsten Carbide tile options

  • Cat GraderBit2™ System

  • End bit systems

  • Ripper/scarifier systems

Wheel Loaders

Caterpillar offers a complete line of edges, tips, adapters and sidebar protectors for more efficient material handling. For high-wear applications, the mechanically attached wear plate system (MAWPS) offers added protection. The total wear protection line offers weld-on heel shrouds and half-arrow edges to protect the bottom and sides of buckets.

of

Abrasion Resistant Material (ARM)

Cat abrasion resistant material (ARM) is a coating made of extremely hard tungsten carbide particles. It forms a protective shield over key wear surfaces, making it ideal for high-abrasion, low-to-moderate impact applications. Those include working in granite, broken slag and other abrasive materials that can severely diminish GET wear life.

How To Maintain Your GET

Ground engaging tools do serious heavy lifting, making maintenance a must. Here are a few steps you can take to optimize the lifespan of your GET.

  • Prioritize inspections and preventive GET maintenance. Preventive maintenance is important for all equipment and attachments because it helps you maintain superior performance. Regular inspection and maintenance help you address minor complications before they become significant, reducing long-term costs.

  • Monitor wear patterns. Uneven wear can indicate an issue with the machine’s operation or alignment.

  • Keep detailed GET maintenance logs. Keep regular maintenance records to ensure you schedule preventive maintenance when necessary.

  • Balance wear. Regularly rotate and interchange parts to ensure even wear.

  • Welding crack repair. If a tool’s welding cracks, it needs immediate repair. Repairing cracks quickly helps prevent further damage so the tool, attachment and machine last longer.

  • Clean regularly. Remove dirt, debris and other material frequently to avoid damage.

  • Operator training. Incorrect operating technique can lead to excessive wear and damage. Properly training equipment operators on operation and maintenance can extend the life of your GET.

  • Know the lifespan of your GET. Ask your Cat dealer about predictive maintenance and technology to help avoid downtime when it’s time to replace your GET. It all depends on the terrain, material and usage for when GET needs to be replaced and how you can maximize the life of your GET.

Still Not Sure Which GET To Choose?

If you have questions about the right GET for your job, consult with your Cat dealer. They can provide expert guidance tailored to selecting the best ground engaging tools for your specific needs.

 

Answers About GET

Q: What are ground engaging tools (GET)?
A: GET are replaceable wear parts like bucket teeth, edges and rippers that help machines dig, grade or move material.

Q: Why go with genuine Cat GET over competitor parts?
A: Genuine Cat parts are engineered to Caterpillar's quality standards. They’re designed to be the perfect fit for Cat machines and attachments and to offer high performance. Additionally, Cat GET are covered by the Caterpillar Usable Life Warranty*.
*where applicable

Q: How do I choose the right Cat GET?
A: Start with the right attachment, then match GET to your application, machine and material. Your Cat dealer can help.

 

 

 

More DIY Articles

Looking for step-by-step instructions for something else? We’ve got you covered.

See More Articles
worker replacing filter in a Cat machine
worker replacing filter in a Cat machine

DIY Maintenance Videos

How-to videos for your most common maintenance needs.

Watch Now
worker inspecting and repairing a machine
worker inspecting and repairing a machine

Parts.Cat.com

All the parts you need for your specific equipment in one convenient place.

Check Out Parts
Cat oils, filters, and greases in workshop
Cat oils, filters, and greases in workshop

 

 

Your Cat Dealer is Standing By

Contact Cat Dealer